Evaluation boards (Discovery or Nucelo) with virtual com port for debugging
Greetings,
I'm new to STM32 MCUs and bought an evaluation board (STM32F072B-DISCO).
I get along surprisingly well, but there is one thing that bothers me:
This combination of MCU (Cortex M0) and ST-Link/V2 seems to lack a virtual COM port for debugging.
I would like to print debug messages to console to inspect complex program flow and read input from console to test program jumps, data processsing and more.
At the moment I connected an USART to my PC with a USB serial interface, but I assumed that the debugger can do this via USB. There seems to be a complex communication protocol for debugging already (live expressions for example) and I wonder why exchanging text messages is impossible.
So I have 2 questions...
Does this board (STM32F072B-DISCO) certainly not offer a solution to print debug messages to a console and read keyboard input without hardware hacks?
Do other boards (Discovery or Nucelo) with ST-LINK/V2-1 or higher and Cortex M3 or higher certainly offer what I'm missing?
Thank you very much and best regards
Jim
Edit: I work with Debian 11 and STM32CubeIDE.