Skip to main content
Visitor II
June 28, 2024
Question

External Interrupt does not turn led on on HAL library

  • June 28, 2024
  • 3 replies
  • 1169 views

Hello, i am trying to run a simple code that toggles the built-in led when i press the built-in user button. I wanted to do this manually using HAL library functions, but for some reason i do not seem to get it right somewhere. The code generated using CubeMX software works, but when i try to code it on my own, i cannot turn the led on. This is the code, and it already is very similar to the code that mx generated. Is there a library or a function that i'm missing?

 

 

#include "stm32g4xx.h"
#include "stm32g4xx_hal.h"

int main(){


	GPIO_InitTypeDef GPIO_InitStruct = {0};
	HAL_Init();

	__HAL_RCC_GPIOC_CLK_ENABLE();
	__HAL_RCC_GPIOA_CLK_ENABLE();

	GPIO_InitStruct.Pin = GPIO_PIN_12 | GPIO_PIN_13;
	GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
	GPIO_InitStruct.Pull = GPIO_PULLDOWN;
	HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

	GPIO_InitStruct.Pin = GPIO_PIN_5;
	GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
	GPIO_InitStruct.Pull = GPIO_NOPULL;
	GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
	HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_RESET);


	HAL_NVIC_EnableIRQ(EXTI15_10_IRQn);

	while(1){


	void EXTI15_10_IRQHandler(void) {
	HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_12);
	HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_13);

	}


	void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) {
	if(GPIO_Pin == GPIO_PIN_13)
	 HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, SET);
	 else if(GPIO_Pin == GPIO_PIN_12)
	 HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, RESET);
	 }

	}

}

 

 

    This topic has been closed for replies.

    3 replies

    Graduate II
    June 28, 2024

    Why do you have EXTI15_10_IRQHandler inside the while loop? 

    while(1){
    
    
    	void EXTI15_10_IRQHandler(void) {
    	HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_12);
    	HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_13);
    
    	}

    That is already in stm32xxxx_it.c file.

     

    Did you enable the NVIC for that GPIO?

    KarlYamashita_0-1719605466499.png

     

     

    Graduate II
    June 28, 2024

    In your HAL_GPIO_EXTI_Callback you have no debounce routine. See this YouTube video to learn how to debounce a button using interrupt. https://www.youtube.com/watch?v=o0qhmXR5LD0

    Super User
    June 28, 2024

     a simple code that toggles the built-in led when i press the built-in user button.

    Nothing is too simple for a beginner. So let's look at your code again.

    * The code probably does not compile as is because there are nested functions? You cannot run the program unless it compiles without errors.

    * Why two interrupts on pins 12 and 13? You wrote about one "built-in user button". Is it a Nucleo board? What is another interrupt for?