Skip to main content
Visitor II
July 12, 2017
Question

F070F6 Device with Device ID F04x?!

  • July 12, 2017
  • 4 replies
  • 765 views
Posted on July 12, 2017 at 09:01

Hi, I am not sure if it's an proper question to ask here, but I ask it here anyway.

I've got some lovely tiny STM32F070F6P6 (with THIS package information on mcu) from china distributor.

Custom boards are made, chips are mounted.

When I start the ST-Link utility, it gives the following message:

0690X00000602U2QAI.bmp

Is this normal?

Or it's just a cloned F070, but with more functions like F04x?!

#stm32-f0 #st-link-utility #device-id
    This topic has been closed for replies.

    4 replies

    Zt LiuAuthor
    Visitor II
    July 12, 2017
    Posted on July 12, 2017 at 09:28

    I should remark that this presumed F070 is currently running a USB CDC function without any problem.

    Zt LiuAuthor
    Visitor II
    July 20, 2017
    Posted on July 20, 2017 at 04:37

    I've just received my new 

    STM32F070F6P6 from MOUSER ...

    Surprisingly the device ID is still 0x445 which means it's a F04x device.

    I try to build some project for F040 and initialize some peripherals which don't exist in F030, (like I2S),

    amazingly, it's working!!??

    What can I do about this?

    .Zt

    Graduate II
    July 20, 2017
    Posted on July 20, 2017 at 06:09

    ST has been know to ship parts with more advanced die than the marking would suggest. If the F04x is a super-set of the F070 then that is a possibility.

    Visitor II
    January 11, 2019

    0690X000006D4BFQA0.jpgI have problem with STM32 loader as the picture : There is no device number and device ID !