Failed to execute MI command. GDB server doesn't initiate on macos mojave 10.14.6
Hello,
I recently updated my OS (from OSX High Sierra to OS Mojave) and the gdb server stopped working.
Unfortunately there isn't many logs regarding what happened, all I get is an error message in a pop-up window saying that it failed to find the directory "localhost" which is pretty weird and doesn't make much sense to me.
I also attached an image of the pop-up window and my OS version in case it might help. Bellow there is the output of the IDE's console.
STMicroelectronics ST-LINK GDB server. Version 5.2.3
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Has anyone encountered this problem before?