Skip to main content
Visitor II
February 1, 2022
Question

Failed to start GDB server

  • February 1, 2022
  • 2 replies
  • 906 views

Hello, I have been trying for a while to test the STMCube programming chain up to the STM32F411 via the STLink without success despite all the ideas read in the forum. During a review of the requirements for the installation of CUBE it is noted, under Windows, WIN 7, 10 but not 8 or 8.1. Too bad, 8.1 is my OS. I attach the error message that it returns to me systematically. Thanks for your help !

Error in final launch sequence: Failed to start GDB server

Error in initializing ST-LINK device.

Reason: (17) Could not find an ST-LINK with serial number 310061000E00004637364D4E.

Please verify the serial number in the debug c

PS: the serial number is the same as the one present when opening STM32 LINK utility

    This topic has been closed for replies.

    2 replies

    Technical Moderator
    February 1, 2022

    Hello

    It is an STM32F411 Discovery board ?

    Can you connect to the F411 with the ST-Link Utility ?

    FranckenoAuthor
    Visitor II
    February 4, 2022

    Hello, no I am using STM32f411 black pill. And yes I can connect without problem with STM Link utility. Have a nice day and thank you