Flashing a blank STM32
I have an STM32L4R5ZI-P on a custom PCB. When designing the PCB I did not think far ahead enough and do my due diligence when it came to assigning and wiring pins on the STM32 in order to flash it. My design incorporates USB D connected to my PCB which supplies power, and such, along with connections to USB_DM and USB_DP on my STM32. I did not wire BOOT0 or NRST. After looking online a bit, I heard that I must pull BOOT0 high and NRST low, allowing the STM32 to enter boot mode and then I can flash my STM32 via the DM and DP pins (using the CubeIDE and CubeProgrammer, etc.). I was just planning to jump BOOT0 to 3.3V and NRST to GND and then use my DM and DP pins on the USB to program is somehow using my PC. Am I thinking about this correctly? Is there an easier way to flash my virgin STM32 on my custom PCB? I do have a NUCLEO evaluation board for my specific STM32L4, which I have programmed and ran code on already. I was wondering if I can utilize the ST-LINK that is on the NUCLEO board to flash the virgin STM32 on my custom PCB. Any advice or pointers will help. Thank you