G431needs hard reset after power-up (Nucleo-32)
Heyho,
I'm working with a STM32G431 on a Nucleo-32.
I've played with it before some years ago, so I already put on a 24 MHz crystal "HSE".
I'm using only the in-built ST-Link's USB power as a source.
Problem:
after connecting USB, the reset button must be toggled to start the controller.
Any ideas how this can be prevented?
We want to use the Nucleo for some in-house testing, and it would be nice if the controller started instantly at power-up without the reset button (which might be "hidden" in a small case).
Google and search here didn't really show this problem.
Thanks!