generate one 10-microsecond pulse followed by fifteen 2-microsecond pulses
Hi,
I want to generate a timeslot control signal consisting of one 10-microsecond pulse followed by fifteen 2-microsecond pulses.
I want the period to remain constant, aligned on the falling edge.
My problem is that before and after the long pulse, the period changes, and I don’t know how to fix it.
I have:

instead of:

I use two methods and i am not able to make both of them work.
Here is my code:
Method 1 : Timer1 16 in PWM mode
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
if( htim->Instance == TIM16)
{
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_5, GPIO_PIN_SET);
else
{
if(htim->Instance->RCR>0)
{
htim->Instance->RCR=0;
htim->Instance->CCR1=g_TSC_Long_Low_Pulse_Duration-1;
}
else
{
htim->Instance->RCR=(g_TSC_Max_TimeSlotsToRun-1)-1;
htim->Instance->CCR1=g_TSC_Short_Low_Pulse_Duration-1;
}
}
}
}
Method 2: time base (Tim 6)
typedef enum {
PULSE_LOW,
PULSE_HIGH
} PulseState;
PulseState pulse_state = PULSE_LOW;
uint8_t ts_counter = 0;
bool is_long_pulse_done = false;
g_TSC_Full_Signal_Period = (uint32_t)((double) (1/((TS_ACQ_RATE_HERTZ) / HAL_RCC_GetSysClockFreq()) ));
g_TSC_Short_Low_Pulse_Duration = (uint32_t)((double) (TS_SHORT_PULSE_DURATION_S * HAL_RCC_GetSysClockFreq()) );
g_TSC_Short_High_Pulse_Duration = g_TSC_Full_Signal_Period - g_TSC_Short_Low_Pulse_Duration;
g_TSC_Long_Low_Pulse_Duration = (uint32_t)((double) (TS_LONG_PULSE_DURATION_S * HAL_RCC_GetSysClockFreq()) );
g_TSC_Long_High_Pulse_Duration = g_TSC_Full_Signal_Period - g_TSC_Long_Low_Pulse_Duration;
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
if (htim->Instance == TIM6)
{
switch (pulse_state)
{
case PULSE_LOW:
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_RESET);
if (!is_long_pulse_done)
__HAL_TIM_SET_AUTORELOAD(htim, g_TSC_Long_Low_Pulse_Duration-1); // long LOW
else
__HAL_TIM_SET_AUTORELOAD(htim, g_TSC_Short_Low_Pulse_Duration-1); // short LOW
pulse_state = PULSE_HIGH;
break;
case PULSE_HIGH:
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_SET);
if (!is_long_pulse_done)
{
__HAL_TIM_SET_AUTORELOAD(htim, g_TSC_Long_High_Pulse_Duration-1); // long HIGH
is_long_pulse_done = true;
ts_counter = 0;
}
else
{
__HAL_TIM_SET_AUTORELOAD(htim, g_TSC_Short_High_Pulse_Duration-1); // short HIGH
ts_counter++;
if (ts_counter >= 15){
is_long_pulse_done = false;
}
}
}for the second method i have an extra problem, i can not have a pulse with less then 3 micro second width
Can somebody help me please?