GPIO output level consistency issue
Hello,
I have three GPIOs output configured. I'm having some strangeness on two of these that I don't quite understand.
I'm using a nucleo STM32L432KC, and I have some custom circuitry attached to the GPIOs (detailed below)
The situation I am experiencing is as follow.
When I set the 3 GPIOs like so, I have expected results.
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_7, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_SET);
PB7,PA5 are low and PA6 is high.
The next condition I test:
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_7, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_RESET);Should show PB7 low, PA5 high ad PA low.
But instead I see this:
PA5 appears to be bouncing all over the place, and once in a awhile PB7 does as well.
(This is short sample, of like 5 seconds)
Finally, when I do this:
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_7, GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_RESET);I see these results:
Both PB7 and PA5 are high, and steady.
Each circuit is tied to a 10k pulldown resistor.
PA6
PA5
PB7
I don't quite understand a) why won't PA5 stay up, and how is PB7 somehow tied to PA5.
If anyone has some ides, I'd appreciate it.