Grid connected inverter with STM32H747I-DISCO
I would like to use STM32H747I-DISCO for grid-connected 3-phase converter applications. The reference command will be provided over an Ethernet port. That means control and connectivity are required for my application.
Can I use the STM32H747I-DISCO board for this purpose?
This board has a built-in Ethernet port. However, I did not find any specifications for the PWM and ADC pins.
Although the MCU has all of these features, does the board have an accessible pin for PWM and ADC functions?
I was looking for some STM32 products that give me similar features, like the C2000 F28388D control card.
I am very impressed with the STM32CUBEMX features.
Please guide and advise.
Regards
Ismail