H753ZI - PIN A2 - ADC
Hi,
I'm using the H753ZI board with 26 ADC inputs on ADC1 & ADC3.
The ADC pins run in DMA circular mode and all inputs seem to work fine except one pin: PA2
PA2 is configured like the other pins: Analog mode, no pull-up and no pull-down

But the pin seems to be connected to the 3V3 pin on CN11. There is only a 1.5k resistance between the two pins, so it looks like it's in pull up mode. When PA2 is not connected to anything, it's at 3.3V. How could this be? Should I put it in pull down mode? Should I connect an external pull down resistor?
I'm driving the ADC pins with an opamp in voltage follower mode as a buffer. With 0V input on the opamp +in, the output of the opamp and pin PA2 go to 0.25V. I'ts not that big of a problem, the ADC still works but it lowers the sensitivity of that pin
I have two boards and both show the same behavior on PA2 (with the same software, so it might be a bug in my software).