H755 UART issue Data corrupted with same baud rate
Hi all,
I'm using Nucleo H755 I have configured UART with 115200 baud rate and the Rx in Interrupt mode
issue: While the STM is configured with 115200 baud rates, when I transmit some data with the same baud rate either the data is corrupted or data is not read/ transmitted, if I reduce the baud rate of the other device by 3 times the baud rate set in ST the Data is read properly. if anyone have any solution regarding this issue, please let me know in this thread I have checked with different STM ide versions, different H755 boards I'm facing this same issue
also, I have checked with H723 which is working fine for the same setup. there are different issues with the H755 boards. also, if anyone from STM team finds this message I'm also facing a issue while reconfiguring the ioc file from cube ide some pins get reset every time
If any other details required, please feel free to ping me