HAL ECC error is not being acknowledged by __HAL_FLASH_GET_FLAG(FLASH_FLAG_ECCR_ERRORS)
I am running into an ECC error when writing to flash when the device is powering down - unfortunately this is a state I cannot control. In the NMI handler when the device boots up I read through the flash and an ECC error pops up and the NMI Handler is triggered. In my NMI handler checking __HAL_FLASH_GET_FLAG(FLASH_FLAG_ECCR_ERRORS) is not returning any flags, but READ_BIT(FLASH->ECCR, (FLASH_FLAG_ECCR_ERRORS)) is returning a flag. Why is this is it a bug with the HAL?
I am on a stm32l476rc currently using HAL 1.11.1.0