Question
How can i output 5V from the STM32303E-EVAL board. By default it can only output 3.3V.
For my project, i need to power a relay that works on 5V. But the outpout available to me from the board is only 3.3V and due to which it is not enough to power on the relay.
There is a D5V pin on the CN6 connectors, but it does not give out 5V.
do i need to change some jumper settings ? or do i need to write that pin high to enable 5V ?