Question
How can i set baud rate greater than 115200 for virtual com port?
I'm now using NUCLEO-L476RG. My PC connects to the board by virtual com port? And i try to set a baud rate greater than 115200 but the data received from usart2 is wrong. However, when i set the baud rate less than 115200, it works well.
So i wanna ask that if 115200 is the upper limitation of virtual com port? If not, how can i set a higher one?