Skip to main content
Explorer
September 6, 2024
Solved

How do I drive the Nucleo_F722ZE board with the STLINK board removed?

  • September 6, 2024
  • 2 replies
  • 2077 views

Hi, everyone.

I cut the stlink board from my Nucleo-F722ZE board.

And I supplied 5V power through E5V of CN11 And JP3 was set to E5V.

I confirmed that the PWR LED was on.

But the embedded program did not run.

I confirmed that this Nucleo-F722ZE board receives MCO input from the STlink board. But now there is no stlink board on my Nucleo.

So, I decided to use the HSI clock rather than the HSE clock.

I set "HSE not used" according to the manual.

 

- SB148 and SB163 ON

-SB112 and SB149(MCO) OFF

-SB8 and SB9 removed

 

And  I enabled HSI in cubeIDE's clock setting.

chulhoolimnnftech_0-1725608565996.png

chulhoolimnnftech_1-1725608601626.png

 

My embedded program on my nucleo runs. But it stops at HAL_Delay().

What part is the problem?

Is the way I did it correct?

    This topic has been closed for replies.
    Best answer by mƎALLEm

    Thanks,

    Just disable USB and all goes fine.

    SofLit_0-1725614172277.png

    PS: USB needs to use HSE with an external crystal. That's why you are having this message.

    2 replies

    Technical Moderator
    September 6, 2024

    Hello @chulhoolim-nnftech and welcome to the community.

    According to the image you shared there is something going wrong in your RCC config. You have an error in the configuration:

    SofLit_1-1725612474224.png

    What message do you get when you pass the mouse cursor on the red square of HSI selection?

    Explorer
    September 6, 2024

     

    chulhoolimnnftech_0-1725613096467.png

     

    Thank you for your reply.

    The message is "PLL Mux should have HSE as input"

    But My nucleo board doesn't have an input oscillator. 

     Can't I use that "HSE not used"?

    Technical Moderator
    September 6, 2024

    Could you please share your ioc file?

    Explorer
    September 6, 2024

    Ah. I pressed wrong " Accept as Solution" button. Sorry. 

    Anyway Thank you very much!