Skip to main content
Visitor II
September 26, 2019
Question

How do I fixed it? "init mode failed"

  • September 26, 2019
  • 1 reply
  • 1927 views

Dear, you

About 6 month ago, I join class for ARM core.

It very interesting for me.

So I made customized PCB with STM32F429ZI Core.

Before when I made customized PCB, I study for nucleo board.

I testing my made PCB Board, I look problems.

The test environment is below:

Computer : windows10 Home x64

Program : System Workbench for STM32

Debugger : ST link V2

Error MSG

Info : Listening on port 666 for tcl connections

Info : Listening on port 444 for telnet connections

Info : clock speed 8000 kHz

Info : STLINK v2 JTAG v34 API v2 SWIM v7 VID 0x0483 PID 0x3748

Info : using stlink api v2

Info : Target voltage : 3.206299

Error : init mode failed (unable to connect to the target)

in procedure 'init'

in procedure 'ocd_bouncer'

I generated code, used CubeMX.

Debugger used JTAG port(20pin).

I already tried STM32 ST-LINK Utiltiy, but situation is same(ST-Link V2 Firmware update included).

I don't konw why this happend, and It make me crazy.

Anyone help me please.

If anyone want to see a schematics, I'll upload.

Thank you.

    This topic has been closed for replies.

    1 reply

    Graduate II
    September 26, 2019

    Check voltage present on NRST and VCAP pins

    YKang.9Author
    Visitor II
    September 26, 2019

    0690X000009jHLRQA2.png

    Here my schematic capture files atttached.

    NRST Pin check oscilloscope

    Power on : NRST near 0 voltage

    System Workbench for STM32 program debug image click : NRST near 3.3 voltage

    You'll see about a VCAP.

    In my schematic, VCAP1, VCAP2 is conneected GND.

    Thank you.