Question
How do I have to configure the standard debug PINS (PA13 and PA14) on STM32F030F4P6 if I want to use them as GPIO output?
Currently I only set the MODER register to 0 and set the outputs to 0 with the BRR register since I don't need further configurations. I allready use other PINs with the same configuration and they work. I read that this should work, but on my HW it doesn't.