How to distinguish multiple Nucleo "removable drives"?
When you plug a Nucleo board into a Windows PC, it pops up as a removable drive - with the drive name helpfully set to identify the type of Nucleo; eg,
Which is great if they are different types of Nucleo.
Not so much if you have more than one of the same type:
So how can we tell which one is which when we have more than one of the same type?
The Drive letter is no use - as that can change.
Any changes to the label are not saved - it reverts to default next time the board is plugged in.