Skip to main content
Visitor II
January 5, 2026
Question

How to get Tutti Frutti to display on STM32H747I-DISCO

  • January 5, 2026
  • 1 reply
  • 83 views

I have an STM32H747I-DISCO board that I am trying to bring up with the Tutti Frutti Demo.   I have followed the instructions in UM3008 to program this as it appeared to be blank upon arrival from Digikey.    

External loader was set to:  MT25TL01G_STM32H747I-DISCO

Programming of CM4 with intflash.hex and CM7 with target.hex completed successfully.

After programming, the board does not display anything and LD10 just flashes red a couple of times and then pauses on green then repeats.

Power LED is good (green).

 

I am not familiar with these development tools so it is likely I'm missing something but whatever it is is not clear to me.

I have tried resetting both through STM32CubeProgrammer (V2.21.0) as well as hard reset on the board.

Power cycling the board does not help.     LD10 just solid red until I connect up STM32CubeProgrammer at which point it cycles between green and red as described above.    I have seen this is a common issue with this board but I have not found an actual solution to this yet.   If this solution exists, can someone point me to it?

 

Fun note:   I did try to have AI help me with a solution on this.     While entertaining after the fact, not recommended for those easily frustrated as it sent me down dozens of paths while giving incorrect info on quite a bit.  :)

    This topic has been closed for replies.

    1 reply

    WillKAuthor
    Visitor II
    January 5, 2026

    I should have added.   I was able to download and run touchGFX on this board.

    Technical Moderator
    January 6, 2026

    Hello @WillK and welcome to the ST community,


    @WillK wrote:

    I should have added.   I was able to download and run touchGFX on this board.


    From this statement I didn't understand if you have solved the issue or you've just uploaded another TouchGFX example to the board and worked fine but not the Tutti Frutti demo!