How to re-program the ST-Link micro (STM32F103CBT6) on a STM32nucleo evaluation board (MB1136 rev C)
I have a stm32nucleo (NUCLEO-F091RC) eval board
I believe that a student has over written the code on the ST-Link micro (STM32F103CBT6) possible by writing to the Virtual Drive that now appears
It powers up and LD1 flashes but it does not enumerate over USB
I have real ST-Links and other Nucleo boards
How do I reload the code for the ST-Link micro on this board and where can I obtain the code to re-flash
It looks like I can remove the jumpers from CN2 short SB6 (SWCLK) and SB10 (SWDIO) and use an external ST-Link
But where can I get the code to load
Thanks
Joe