Skip to main content
Explorer
May 8, 2024
Question

How to use STM discovery board as external Debugger

  • May 8, 2024
  • 5 replies
  • 1755 views

I have F407G Disc1 board where it has the SWD ports and I want use this board as a standalone external debugger and I went through the manual for the connections but got stuck
Also found a thread in stack exchange where the connections are given as below

Screenshot 2024-05-08 150043.png

Akshay__0-1715161299835.png

 

Where are the pins PA13 and PA14 in SWD here?
It would be really helpful if the name of the respective pins be given here

    This topic has been closed for replies.

    5 replies

    Super User
    May 8, 2024

    Get ST-LINKv3, do yourself a favor.

    Akshay_Author
    Explorer
    May 8, 2024

    I want to know it with V2 
    Can you answer it if possible

    Super User
    May 8, 2024
    Akshay_Author
    Explorer
    May 8, 2024

    Is port 1 PA13
    We have 6 pins here, what does each pin signify here?

    Graduate II
    May 8, 2024

    An easy test is when you have two similar board, best with different CPUs to see the difference. disconnect the jumper on one board and connect SWD pind 1-4  to the other board ST-Link connector. Keep the orientation. No one board should see the other cpu.