how to use UART2 independently - isolated from ST link. STM32103RB
i have STM32103RBT6, i want to use all three UARTs for a project. i want to use UART2 thorugh PA2 and PA3.
The connection are : SB61, SB62 and SB63 are open. SB13 & SB14 are open as well. Continuity is there between SB62 & SB62 to TX on ST link (from track side) & between SB63 to RX on ST link (from track side). No continuity between PA2 and PA3 with SB13 & SB14. can anyone tell me how to use UART2 from the PA2 and PA3? i want to use it for modbus but the transmission is failing.