I am experiencing failures of the LSE oscillator on STM32F427VIT6 during thermal cycling.
I have an ESC ECS-.327-CDX-1082 32.768KHz crystal on the LSE of an STM32F427.
I have read and followed AN2867.
All of the boards produced so far have had the oscillator come up initially.
All of the boards subjected to thermal cycling (-20°C to +70°C) have failed. (two)
In each case, the voltage on the pins (GPIO PC14 & PC15) measures 0 volts.
I expect somewhere about 0.3V.
I just replaced the MCU on one of the boards and now the oscillator works again.
Any thoughts?