Skip to main content
Visitor II
January 20, 2023
Question

I am experiencing failures of the LSE oscillator on STM32F427VIT6 during thermal cycling.

  • January 20, 2023
  • 22 replies
  • 5965 views

I have an ESC ECS-.327-CDX-1082 32.768KHz crystal on the LSE of an STM32F427.

I have read and followed AN2867.

All of the boards produced so far have had the oscillator come up initially.

All of the boards subjected to thermal cycling (-20°C to +70°C) have failed. (two)

In each case, the voltage on the pins (GPIO PC14 & PC15) measures 0 volts.

I expect somewhere about 0.3V.

I just replaced the MCU on one of the boards and now the oscillator works again.

Any thoughts?

    This topic has been closed for replies.

    22 replies

    BRieh.1Author
    Visitor II
    April 13, 2023

    Sorry for the delay.

    It looks as if it takes 2-10msec after the backup domain reset before the LSE is stable.

    Super User
    April 13, 2023

    LSE startup can be long... (from F407 data.)


    _legacyfs_online_stmicro_images_0693W00000bi2cwQAA.png