I can't use the ST-link in STM32CubeIDE even after updating the ST-link firmware
I am trying to debug the STM32C8T6 with st-link and STM32CubeIDE, following errors happened, I need help to solve this problem,
"
STMicroelectronics ST-LINK GDB server. Version 5.5.0
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
The detected ST-Link firmware version does not support the DAP read command
Waiting for debugger connection...
Debugger connected
The detected ST-Link firmware version does not support the DAP read command
-------------------------------------------------------------------
STM32CubeProgrammer v2.4.0
-------------------------------------------------------------------
Error: ST-LINK V1 not supported
Error: ST-LINK V1 not supported
Error: ST-LINK v1 not supported.
Encountered Error when opening C:\ST\STM32CubeIDE_1.3.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.3.0.202002181050\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Debugger connection lost.
"
One thing to mention that I have updated the ST-link firmware to V1J13S4 STM8/STM32 debugger from older version by clicking the menu->help->st-link update