I cannot get high-frequency oscillator to work with STM32F765VGT6 MCU.
I have designed/developed more than 140 microcontroller-based boards utilizing 8, 16 and 32 bit MCU's. I recently designed a board that uses a STM32F765VGT6 MCU. During my initial power-up test, I verified that all of the voltages are in range. However, I have been unable to download any code into the MCU because the J-LINK debugger thinks the device type is incorrect. After many hours of troubleshooting, I discovered that the (25 mhz.) high-frequency oscillator is not working!! I tried 3 different crystals but the problem remains. I spent 8 hours verifying that the pin definitions on the schematic are correct. I have never had this kind of problem in all of my years of working with devices like this. I am attaching the simplified schematic. Any help from a fresh set of eyes would be greatly appreciated!!