I cant connect to my EVALKITST8500-1 using Smartgrid LabTool V4.4.
The power cable and the USB cable for kit interface are connected properly.
When I connect the interface cable as per the the quick start guide, the LabTool does not recognize any port. If I go to settings - port: I can find no port to chooseIf I go to settings - COM port - Scan port: Again, nothing happens.In my windows device manager, I can see two new devices which don't have the appropriate driver, there are named: Enhanced COM port, and standard COM port. #evalkitst8500-1 #smartgrid-labtool