I have a question regarding the STM32L083CZT6 microcontroller. I have designed a custom board using this microcontroller, but it's not working!! Do you have any tips?
I have tested the microcontroller with different boards and all have the same problem.
I have noticed that the voltage across the NRST is 0V, which I think means that the microcontroller is damaged (There is no short circuit in the system).
I have connected the microcontroller to the PC through a serial wire debugger (using STLINK-V3MINI) and it says MC not found.
I have designed a custom board using STM32F4 before and I didn't have a problem before.
Do you have any tips to find the problem?
Thanks
Here is the Circuit design