Skip to main content
Visitor II
March 14, 2024
Question

I2C Communication with STM32U5A9J_DK with LCD 16*2 External I2C device

  • March 14, 2024
  • 1 reply
  • 591 views

How to implement I2C communication between STM32U5A9J_DK board with external LCD 16*2 I2C device 

    This topic has been closed for replies.

    1 reply

    Technical Moderator
    March 14, 2024

    Hello @ManasaPK and welcome to the ST Community :smiling_face_with_smiling_eyes:.

    I don't think there is a specific Firmware for communication between STM32U5A9J_DK with LCD 16*2 External I2C device. What I suggest you is to migrate one of the available examples on the internet or YouTube using STM32F4 or other boards for examples. But why are using the external LCD 16*2? our discovery board integrate a 2.47‑inch RGB 480 × 480 pixels TFT round LCD module which you can use for a very good displaying experience:

     

    STTwo32_1-1710400703026.jpeg

    Best Regards.

    STTwo-32