I2C pin voltage is at 3.5V
I'm using the i2c on a nucleo stm32h723 board. I'm using pins PB8 and PB9 on the board. I have the pins connected to a scope. I notice that when I have the internal pullups of the board on the voltage is at 3.5V and if I dont use the internal pullup, then the voltage is at 3.5V then drops to 3.3V. Was wondering if the pins are broken or if the jumpers on the board are inncorrect since the i2c line should be at 3.3V even with internall pullup.