Skip to main content
Visitor II
August 22, 2024
Solved

Interfacing PS2 controller with STM32F103RBT6

  • August 22, 2024
  • 1 reply
  • 1493 views

Hi, I am trying to interface a PS2 controller with a STM32F103RBT6 board and I'm relatively new to STM32 in generally. I have understood how the PS2 protocol works and was able to find references with codes to run with. Unfortunately, the board configuration in the ioc file of the given by the reference is of a STM32F103C8Tx board(surprisingly it operated successfully on my RBT6 board and was able to get the key input readings), and the key input reading are not reflected properly when running the codes (with only changes to microsecond delay functions) with a STM32F103RBTx board configuration.

Is there any explanation and solution to this? Any help is greatly appreciated!

Full files of the PS2 controller interfacing code is attached to my google drive in the following link. ("PS2" folder is for C8Tx version, "PS2_RBver" is for RBTx version)

https://drive.google.com/drive/folders/1BYTq7MRy8VRNGXaSP2vrUbU0-paIUpZd?usp=sharing

 

    This topic has been closed for replies.
    Best answer by Mike_ST

    Hello,

    In the RBT6 project clock configuration, the APB2 prescaler is set to 2, when it is 1 in the CBT6 project.

    You're using the TIM1 which is on the APB2 bus, and with the same settings for prescaler and counter period in both projects.

    So whatever you're doing with TIM1 might be wrong.


    Also, the PS2_AnologData() in not the same in the 2 projects.


    For the delay function, you might want to stick to the working one of the original project.

    1 reply

    Mike_STAnswer
    Technical Moderator
    August 23, 2024

    Hello,

    In the RBT6 project clock configuration, the APB2 prescaler is set to 2, when it is 1 in the CBT6 project.

    You're using the TIM1 which is on the APB2 bus, and with the same settings for prescaler and counter period in both projects.

    So whatever you're doing with TIM1 might be wrong.


    Also, the PS2_AnologData() in not the same in the 2 projects.


    For the delay function, you might want to stick to the working one of the original project.