Is it mandatory to cut off the Nucleo board in order to use PA13 and PA14 to program with ST-Link/v2?
Hi everyone,
I play with a Nucleo-F767ZI, using the ST-Link part provided on the PCB.
I would like to use a ST-Link/v2 to program my MCU.
I was wondering, whether it is possible to power my MCU (without USB PWR) and use the ST-Link/v2 (using PA13 and PA14), without cutting the ST-Link part of the Nucleo or removing other components off the board.
UM1974, on page 71, says:

and:

My guess would be, I can't, but I don't understand why?
Do you have an explanation?
Cheers,
Ced.
#nucleo-f767zi #st-linkv2