Skip to main content
Visitor II
June 7, 2022
Solved

Is it mandatory to use an external DC/DC converter with STM32L496 with external SMPS package? Or would it just affect the consumption in run modes?

  • June 7, 2022
  • 1 reply
  • 1122 views

I would like to know if the micro can work exclusively with the internal LDO for the Vcore

    This topic has been closed for replies.
    Best answer by Peter BENSCH

    Welcome, @ILobo.1​, to the community!

    The external SMPS is intended exclusively for the possibility of maximum energy saving if you supply the STM32 e.g. via a battery or from an energy harvester.

    Of course, you can use the STM32L496 without an external SMPS and only with an internal LDO, but then you will burn up considerably more electrical energy, as you can see from the corresponding parameters in the data sheet.

    Does it answer your question?

    Regards

    /Peter

    1 reply

    Technical Moderator
    June 7, 2022

    Welcome, @ILobo.1​, to the community!

    The external SMPS is intended exclusively for the possibility of maximum energy saving if you supply the STM32 e.g. via a battery or from an energy harvester.

    Of course, you can use the STM32L496 without an external SMPS and only with an internal LDO, but then you will burn up considerably more electrical energy, as you can see from the corresponding parameters in the data sheet.

    Does it answer your question?

    Regards

    /Peter

    ILobo.1Author
    Visitor II
    June 9, 2022
    Yes, it answers my question. Thanks!
    Technical Moderator
    June 9, 2022

    Great!

    If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

    /Peter