Skip to main content
Visitor II
June 26, 2022
Question

Is it possible to use ST-LINK/V2 from a Windows 11 machine?

  • June 26, 2022
  • 2 replies
  • 1908 views

Hello,

Is there a way to use a ST-LINK/V2 from a Windows 11 machine? The device is not recognized when I connect it to the computer. The specifications indicate that the official support does not exceed Windows 10. The latest drivers have successfully been installed on my computer but the ST-LINK/V2 is not recognized. I tried to manually install the .inf file too, but to no avail.

EDIT: I got it to work by programming my board via a STM32F1 Discovery board (used as a programmer) circumventing the ST-LINK/V2 entirely.

    This topic has been closed for replies.

    2 replies

    Graduate
    June 26, 2022

    Yes, it is fully supported. Just install the current driver supplied with STM32CubeIDE or STM32 CubeProgrammer, not the old stuff from .zip files. Are you sure you have the legitimate ST-Link? The ST drivers may detect the hacked serial number and refuse to work with illegal clones.

    Visitor II
    June 27, 2022

    Thanks for your reply.

    I started with an installed STM32CubeIDE/Programmer that did not work, later I did indeed install the .zip file you mentioned. My ST-LINK/V2 used to work before I upgraded to Windows 11. No idea, though, whether it is a legitimate device.