Skip to main content
Visitor II
December 14, 2017
Solved

Is nucleo_l152re a two layer (or more) PCB design?

  • December 14, 2017
  • 1 reply
  • 989 views
Posted on December 14, 2017 at 18:57

I see there some have problems (the board doesn't work well anymore) after separating the programmer part from the rest of the board. And I intend to use this tool to cut the bridges...

0690X0000060PGVQA2.jpg

#pcb #cut #bridges
    This topic has been closed for replies.
    Best answer by Tesla DeLorean
    Posted on December 14, 2017 at 19:06

    Load the Gerbers into a viewer?

    http://www.st.com/resource/en/board_manufacturing_specification/nucleo_64pins_gerber.zip

    1 reply

    Graduate II
    December 14, 2017
    Posted on December 14, 2017 at 19:06

    Load the Gerbers into a viewer?

    http://www.st.com/resource/en/board_manufacturing_specification/nucleo_64pins_gerber.zip

    Visitor II
    December 14, 2017
    Posted on December 14, 2017 at 19:20

    So two layers... thank you Clive! There may be several chances to have bridged traces on the bottom layer on a rough cut, and one for the top layer...

    I recommend to make those PCB bridges wider and the traces with more space between them.

    Or on the microcontroller board, 0 ohm resistors as a bridge for the signal traces, that can be un(de)-soldered to avoid short circuit after a separation.