Question
is there an ST-LINK V2 with the V2-A version firmware?
Posted on June 22, 2016 at 11:18
Hi,
Does anyone know if there is an ST-Link (the actual small white unit) that runs the V2-A firmware that allows the Mass storage option? I have an STM32F407G-DISC1 with this feature (with ST-LINK/V2-A only) and it's great. However I have a custom board coming back and now need to use the external unit. It is possible to upgrade the firmware in the ST-Link? Many Thanks, Dirk Vermaak #st-link #stm32f4