Issue on Stm32F429ZI Discovery Board STlink for External Programming/Debugging
I have been using stm32f429 Discovery board for a while. recently i tried to use it for programming a blue pill using onboard St-link v2. But it wasn't working even though all connections are okay. Later i figured figured out that target VDD pin which suppose to return the target voltage to St-link MCU has a unfitted resistor R13 footprint. I checked the schematic and it says the R13 is unfitted. As a result the target VDD pin is totally separated from st-link MCU.
So whats the remedy? should i bridge it? It seems it requires a current limiting resistor. If so what should be the value?