Skip to main content
Visitor II
March 3, 2025
Solved

Issue with V_BAT Connection on Custom STM32F407VGT6 Board

  • March 3, 2025
  • 3 replies
  • 1671 views

Hello everyone,

I have designed a custom board using the STM32F407VGT6, and I have connected a 3V coin cell battery (CR2032) to the V_BAT pin as shown in the schematic below:

V_BAT Circuit Details:

  • A 3V battery is directly connected to the V_BAT pin.
  • A 0.1µF capacitor (C14) is placed across V_BAT and GND.
  • V_BAT is connected directly to the STM32.

However, I am facing an issue where I do not measure any voltage at the V_BAT pin on my board. It seems like the battery is not supplying power to the backup domain.

  1. Why am I not getting voltage on the V_BAT pin?
  2. Are there any hardware design issues with my schematic?
  3. Is there any special configuration required in firmware to enable the backup domain power?

I have attached my schematic for reference.

    This topic has been closed for replies.
    Best answer by TDK

    > do not measure any voltage at the V_BAT pin on my board

    A multimeter across the battery should show voltage. If using the ADC, show relevant code. Should be getting something. Nothing wrong with the schematic snippet.

    3 replies

    Technical Moderator
    March 3, 2025

    Hello,

    You can refer to the STM32F4G EVAL schematics:

    As you can see nothing special:

    mALLEm_1-1741008002938.png

    For the code you can refer to the RTC calendar example here.

    TDKAnswer
    Super User
    March 3, 2025

    > do not measure any voltage at the V_BAT pin on my board

    A multimeter across the battery should show voltage. If using the ADC, show relevant code. Should be getting something. Nothing wrong with the schematic snippet.

    Super User
    March 3, 2025

     

    You can paste the image directly into the post - where we can see it:

    AndrewNeil_0-1741012784009.png


    @rohithinthingstech wrote:

    I do not measure any voltage at the V_BAT pin on my board. It seems like the battery is not supplying power to the backup domain.


    Is the battery dead?

    Have you measured to see if current is being drawn from the battery?

     

    @rohithinthingstech wrote:

    I have designed a custom board .


    Have you checked the layout for shorts?

    Have you checked the assembly for shorts and bad joints?