Issues with connecting with st link board to stm32f103c8t6(Update)[resolved]
So I just recently got an stm32f103c8t6, and I was able to connect to it with the serial pins connected to pins A8 and A9, but for whatever reason, I was not able to get it to connect with the St link v2 that I also ordered. For connections, I connected 3v pin to pin 1, as labeled in the user manual for the st link, ground to 20(power was working and the onboard power LED was on), SWIO to 7 and SWCLK to 9. I was unable to find a video of someone using the official st link online, as basically every video used a knockoff board. Is there something I'm not doing right?
Update, I was able to connect with stm32cubeprogrammer, but not write. I am able to connect with these settings:
SWD
4000khz
hot plug
software reset
I can see the contents of the memory, but I am not able to write to them. Can someone explain what I am doing wrong?