JTAG on the NUCLEO-G474RE, No device found on target.
Hello,
I have an issue with the Nucleo-G474RE, I can't get the JTAG to work, I tried JTAG in 4-pin and 5-Pin-Mode, the IDE reports "No device found on target". With SWD it works in ST-Link-GDB-Server-Mode, but not JTAG. I checked JTAG is connected to the onboard StLinkV3 in 5 Pin JTAG-Mode, seems to be fine.
Does someone know the problem, or may can give me some hints on how to solve that issue?
Thank's a lot in advance.
Best Regards, Seppel
Solder-Bridges still in factory Setting:
SB40 - Set(closed)
SB41 - Set(closed)
SB15 -Set(closed)
SB9 - Set (closed)
SB1 - Set(closed) 100nF from NRST to GND
JP3 -Set(closed)
Console:
STMicroelectronics ST-LINK GDB server. Version 5.8.0
Copyright (c) 2020, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
InitWhile : Enabled
Target no device found
Error in initializing ST-LINK device.
Reason: No device found on target.
Message:
Error in final launch sequence:
Failed to start GDB server
Failed to start GDB server
Error in initializing ST-LINK device.
Reason: (4) No device found on target.