Skip to main content
Visitor II
January 25, 2019
Question

JTAG/SWI pull-up pull-down resistor

  • January 25, 2019
  • 2 replies
  • 2181 views

good morning, I wanted to ask a simple question.

I'm drawing the schematic of a small board based on the NUCLEO-F401RE.

I have a doubt about the JTAG/SWI connector, practically on various schemes I have seen that there are pullup/pulldown resistor (see attached) but on the NUCLEO scheme it seems to me that there are not. So the question is: do I need pull-up/pull-down on the JTAG/SWI interface?

Thanks in advance

 FM

    This topic has been closed for replies.

    2 replies

    Graduate II
    January 25, 2019

    I general you don't need Jtag Pull Up/Down. The STM32 Jtag interface has internal pulls.

    Visitor II
    January 28, 2019

    the SWD interface also have internal pull-up/down ?

    in all cases do you advise me to provide pull-ups on the pcb and not to mount the resistances or is it totally useless and I do not even plan them?