Linux cannot set up ST-Link
Hello,
I am trying flash my STM32F746G Discovery board with new code from Linux. I run into this issue after running "dmesg -w": "can't set config #1, error -32". ST-Link is not being detected by either STMCubeIDE and STMCubeProgrammer. Has anyone run into this issue before?
Furthermore, I had code flashed to the Discovery board that had a screen show, but I am met with a black screen when I connect it to power. The LED next to the ST-Link flashes red. I've also tried changing my debugger from ST-Link to SEGGER, but I met with the error "Could not determine GDB version using command: arm-none-eabi-gdb --version," and I am currently looking into this.
I'm hoping that this is not a board issue but rather a software issue, but at this point it seems like this may be a board issue.
Regardless, has anyone had any issues like this, and can provide any tips on what to do from here?