Skip to main content
Visitor II
December 19, 2024
Solved

Looking for STM32H745II ST board to evaluate ADC

  • December 19, 2024
  • 1 reply
  • 685 views

Hi,

I would like to evaluated ADC of STM32H745. I would like to have 12bit 5.12MHz dual ADC. According to my understanding, I need to use model STM32H745II in 176 pin UFBGA to obtain ADC performance. Is there any board like nucleo, which can be used for evaluation?

    This topic has been closed for replies.
    Best answer by mƎALLEm

    @mosamasa wrote:

    According to my understanding, Disco is based on STM32H745XI (240pin TFBGA). Maximum ADC rate would be only 4.38MHz.


    Yes you're right according to the AN5354:

    SofLit_0-1734618806165.png

    But, unfortunately, there is no other ST boards for STM32H745 with other packages.

    The only available ST boards for STM32H745 are with LQFP144 and TFBGA240.

    1 reply

    Technical Moderator
    December 19, 2024
    mosamasaAuthor
    Visitor II
    December 19, 2024

    According to my understanding, Disco is based on STM32H745XI (240pin TFBGA). Maximum ADC rate would be only 4.38MHz.

    mƎALLEmAnswer
    Technical Moderator
    December 19, 2024

    @mosamasa wrote:

    According to my understanding, Disco is based on STM32H745XI (240pin TFBGA). Maximum ADC rate would be only 4.38MHz.


    Yes you're right according to the AN5354:

    SofLit_0-1734618806165.png

    But, unfortunately, there is no other ST boards for STM32H745 with other packages.

    The only available ST boards for STM32H745 are with LQFP144 and TFBGA240.