Low consumption NucleoL476RG
Hello community, I have been working with the nucleol476rg in low power modes, but I have had some doubts during the tests I have performed, specifically using the stand by mode, I understand that only the RTC is active in fact with it I set the alarm to wake it up from sleep mode, but it does not consume what is specified in the data sheet since it must be below the order of 50uA but depending on how I feed it it consumes 330uA or almost 4mA, 330 when I connect the power to AVDD and 4mA when I connect it to VIN, should some configuration be done from the Firmware or is it some change in the Hardware that must be implemented? I am attentive to any information, thank you very much.