Low Power Reset Circuit
Hello,
Could anybody please look at the circuit, and if it is correct.
I am not sure if C5 is necessary to be there.
Thank you.
Hello,
Could anybody please look at the circuit, and if it is correct.
I am not sure if C5 is necessary to be there.
Thank you.
The reset devices were not developed as an addition to the STM32, but for other devices that still need an external reset and that too with the old method of a pull-up, as was often used in the last century.
In this respect, the internal pull-up is nice, but redundant in the context of the STM32 - as, by the way, is the external reset device. All STM32s have a comparable reset circuit and external pull-ups are redundant on the NRST.
At NRST you only need the 100nF capacitor, if you also want to trigger a manual reset, you can also connect a button - preferably with a 100 ohms series resistor to protect the button contact.
Regards
/Peter
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.