LSCO CLK in pin (PA2) in Nucleo Board G474RE not present
I have tried to route the LSI clock to PA2 pin in my Nucleo Board G474RE without success. SB13 & SB17 are open (it means ST Link is not connected to PA2 pin). Configuration was carried out with STMCube32 Mx but I don´t obtain the CLK in PA2. I have checked also the LSCOSEL and LSCOEN bits and are correct configured.
My dudes are:
1) Muss RTC be activated to obtain the desired behaviour? My suposition is NO, because when I route the LSI to MCO pin (PA8) it works fine.
2) did I forget to modify something else in Nucleo Board G474RE?
Thanks in advance!