LSE won't start - Do I have to big capacitors?
Hi!
I'm using FC-12M 32.7680KA-A5 LSE crystal and my STM32F373VBT6 won't start if I'm suing LSE crystal. But if I'm suing LSI crystal, then my STM32 will start.
I have made two(2) boards and both of them LSE won't start.
My suggestions why are:
- To big capacitors
- STM32F373VBT6 is broken
- The crystal is broken
- Bug in STM32CubeIDE 1.6.1
- Crystal is to far away from the MCU
What do you think is the right according to the information below?
My setup looks like this. I'm using 15 pF capacitors because I computed them with the formula:
C = 2(CL - Cs) = 15
Where CL = 12.5 pF is the load capacity of the crystal.
Cs = 5 pF is the stray capacity of the board.
The PCB layout for the LSE crystal. PC15 and PC14 is it mounted at.
I have followed recommended CubeMX setup
I have selected the correct LSE crystal according from the recommendations from ST.
And the crystal information looks like this: