Measuring power consumption of NUCLEO-N657X0-Q using ST probes
Hi,
I'm wondering if there are any recommendations/guidelines when trying to measure power consumption on the Nucleo-N657X0-Q when running a neural network model, both with NPU acceleration and without on the CPU for comparison. I have access to both a X-Nucleo-LPM01A power shield and a STLINK-V3PWR and do not know which one to choose.
Are both options rated for enough power to measure the board? And does any of the two options require removing components, as the board is borrowed so I would prefer a non-invasive solution.
Thanks in advance!