Missing PG11 on Nucleo UM2581 Board
Hi All,
Is there an errata for the STM32L5 Nucleo board?
I need to use the SPI on port G which requires PG11 for SPI MOSI.
However in the schematic for the board, PG11 is missing from the schematic symbol (see page 3) and there is a gap. The pin numbers in the symbol keep incrementing though.

PG11 is also missing from the Nucleo Pinout table (page 39).

In the STM32L552xx datasheet (page 86), PG11 is assigned 126.

Thank you